This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: How to initiate a soft boot.

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642, AWR1642

I need to be able to have the sensor reboot itself if there is no serial port activity.  Is there a sample or an api call to to reboot.  On the 2640 I called SysCtrlSystemReset();  Which directly wrote to registers.  Is there an equivalent function for the IWR1642?

Also, is there a way to initiate a reboot via the usb port.  Is there some command that i can issue via serial port to reset the unit via XDS110.  In the documentation, it states that the XDS110 uses SW2 (a hardware switch) to reset the unit.  How can i externally make this happen via USB.