Hi,
I am trying to calculate the maximum distance given an ADC sampling rate of 2500ksps and frequency slope of 60 MHz/us. The Dmax is given by (ADC sampling rate * C)/Slope from the Introduction 1.1 video. I get a dmax of 12.49 meters from the above parameters but according to the chirp database's case 1 the max range is 5.6 meters. I got the slope and ADC sampling rate from the corresponding cfg file (2500ksps and 60MHz/us). How did they get get 5.6? Or am I doing something wrong? Lastly, can someone also explain/derive their max velocity as well.