Dear all,
Is it possible to configure the awr1642 family device in only receive mode?
Only Tx should be off but internal chirp should be generating for generating the beat.
Is it possible to achive this with this chipset?
I want to make one device Just receives the Signal and process it. It should not transmit.
I will transmit from other device. So I want a device where I can configure for only receive , When required transmit(Normal Radar Operation).
If 66GHz new chipset TI launched right that works for me is also fine enough.
Thanks in advance