Hi Champs,
I believe that the boot loader program which is kept in somewhere in AWR1642 is loaded to MSS and then it runs, after SOP is set 101 ((SOP mode 5) = flash) as programming mode and the deice is powered up.
Am I making sense?
Moreover, if the program is running in MSS, could it output the serial log file when any error occurs?
It would be useful feature to debug the problem when we face.
Best regards,
Hitoshi