This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Can't find the target named 'ti.targets.arm.elf.R4F' along the path

Part Number: IWR1642BOOST


I have troubles in this


**** Clean-only build of configuration Debug for project pplcount_16xx_mss ****
"D:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 clean -O
 
DEL /F  "xwr16xx_pplcount_mss.hex"  "configPkg\linker.cmd" "configPkg\compiler.opt"  "xwr16xx_pplcount_mss.xer4f"
DEL /F "cli.oer4f" "cycle_measure.oer4f" "gtrackAlloc.oer4f" "gtrackLog.oer4f" "mss_main.oer4f" "radarOsal_malloc.oer4f" "task_app.oer4f" "task_mbox.oer4f"
DEL /F "cli.d" "cycle_measure.d" "gtrackAlloc.d" "gtrackLog.d" "mss_main.d" "radarOsal_malloc.d" "task_app.d" "task_mbox.d"
RMDIR /S/Q  "configPkg\"
找不到 D:\ti\ccsv8\workspace\pplcount_16xx_mss\Debug\xwr16xx_pplcount_mss.hex
找不到 D:\ti\ccsv8\workspace\pplcount_16xx_mss\Debug\configPkg\linker.cmd
找不到 D:\ti\ccsv8\workspace\pplcount_16xx_mss\Debug\xwr16xx_pplcount_mss.xer4f
找不到 D:\ti\ccsv8\workspace\pplcount_16xx_mss\Debug\cli.oer4f
找不到 D:\ti\ccsv8\workspace\pplcount_16xx_mss\Debug\cli.d
Finished clean
 
**** Build Finished ****
**** Build of configuration Debug for project pplcount_16xx_mss ****
"D:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 all -O
 
rm -f D:/ti/ccsv8/workspace/pplcount_16xx_mss/xwr16xx_pplcount_mss.bin
makefile:193: recipe for target 'pre-build' failed
process_begin: CreateProcess(NULL, rm -f D:/ti/ccsv8/workspace/pplcount_16xx_mss/xwr16xx_pplcount_mss.bin, ...) failed.
make (e=2): 系统找不到指定的文件。
 
gmake[1]: [pre-build] Error 2 (ignored)
 
Building file: "../mss_mmw.cfg"
Invoking: XDCtools
"D:/ti/xdctools_3_50_08_24_core/xs" --xdcpath="D:/ti/bios_6_75_01_05/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.R4F -p ti.platforms.cortexR:IWR16XX:false:200 -r release -c "D:/ti/ti-cgt-arm_16.9.6.LTS" --compileOptions "--enum_type=int " "../mss_mmw.cfg"
making package.mak (because of package.bld) ...
making package.mak (because of package.bld) ...
subdir_rules.mk:19: recipe for target 'build-1242173169-inproc' failed
js: "./config.bld", line 10: Error: Can't find the target named 'ti.targets.arm.elf.R4F' along the path 'D:/ti/bios_6_75_01_05/packages;D:/ti/xdctools_3_50_08_24_core/packages;..;': please check the spelling of the target's name and that it exists along this path.
js: "./config.bld", line 10: Error: Can't find the target named 'ti.targets.arm.elf.R4F' along the path 'D:/ti/bios_6_75_01_05/packages;D:/ti/xdctools_3_50_08_24_core/packages;..;': please check the spelling of the target's name and that it exists along this path.
gmake.exe: *** No rule to make target `.configuro'.  Stop.
js: "D:/ti/xdctools_3_50_08_24_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake[2]: *** [build-1242173169-inproc] Error 1
gmake[1]: *** [build-1242173169] Error 2
gmake[1]: Target 'main-build' not remade because of errors.
gmake: *** [all] Error 2
subdir_rules.mk:16: recipe for target 'build-1242173169' failed
makefile:159: recipe for target 'all' failed
**** Build Finished ****