Hello,
I wanted to check if there was an easy way to transmit a single frequency using the mmw demo firmware.
What I did is, in the profileCfg, I changed the freqSlopeConst to 0 so:
profileCfg 0 77 916 7 57.14 0 0 0 1 240 4884 0 0 30
The chip is able to accept this configuration but I wasn't sure if it's actually transmitting 77GHz (haven't had a chance to test in lab).
Do you see any issues with this?
Here is the full CFG just in case you need it:
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 2 1 0
adcCfg 2 1
adcbufCfg 0 1 0 1
profileCfg 0 77 916 7 57.14 0 0 0 1 240 4884 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 0
frameCfg 0 0 16 0 100 1 0
lowPower 0 1
guiMonitor 1 1 0 0 0 1
cfarCfg 0 2 8 4 3 0 1280
peakGrouping 1 1 1 1 229
multiObjBeamForming 1 0.5
clutterRemoval 0
calibDcRangeSig 0 -5 8 256
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 123 0
CQSigImgMonitor 0 119 4
analogMonitor 1 1
sensorStart
Thank you,
Faiz