This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Z co ordinate coverage

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: AWR1642,

Hello

1) We are using AWR1642 for short range configuration

Scenario A :  Object(RCS of an adult) is placed  at a height of 1.5 m and radar is placed approx at a height of 1  , radar detects the object .

Scenario B :   Object(RCS of an adult) is placed  on the ground and radar is placed approx at a height of 1 m , radar does not detect the object .

We want to know the z coordinate coverage at a distance of 1.5 m from the radar .

2) In short range radar configuration , could you provide the details of the Tx and Rx beam width  and information on side lobes.

Will these parameters change when the profile is changed .