Hi Experts,
According to the TRM www.ti.com/lit/swru522, the BANK7 for AWR1642 is reserved.
It is shown on Figure 10-2. DSS_L3 Memory Organization in the chapter 10.2.1 Functional Description on page.1167.
On the other hand, it is described in 4.7.1.41 SHMEMBANKSEL7TO4 Register (Offset = 2CCh) [reset = 01010101h].
BANK 7 is allocated to DSS L3RAM (0x01) after the reset.
Let me clarify whether BANK 7 is reserved for BSS TCMA and then a user can not use it.
Or it is depending upon the application so that a user can change the allocation BSS TCMA to BANK 6 instead of 7.
If so, could you please let me know where it is set in our sample code?
Thank you for your kind check.
Best regards,
Hitoshi