This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Repeated control commands

Part Number: IWR6843ISK


I was reviewing the control commands sent when using the the OOB SDK demo (attached below) and I noticed that couple commands were repeated with different arguments. I am not really clear if this intentionally done and why?

% Carrier frequency     GHz                          60.25
% Ramp Slope    MHz/us                               156
% Num ADC Samples                                    256
% ADC Sampling Rate Msps                             12.5
% ADC Collection Time   us                           20.48
% Extra ramp time required (start time) us           3
% Chirp time (end time - start time)    us           21
% Chirp duration (end time) us                       24
% Sweep BW (useful) MHz                              3194.88
% Total BW  MHz                                      3744
% Max beat freq (80% of ADC sampling rate)  MHz      10
% Max distance (80%)    m                            9.62
% Range resolution  m                                0.047
% Range resolution (meter per 1D-FFT bin)   m/bin    0.047
%                                                    
% Inter-chirp duration  us                           7
% Number of chirp intervals in frame    -            64
% Number of TX (TDM MIMO)                            2
% Number of Tx elevation antennas                    0
% Number of RX channels -                            4
% Max umambiguous relative velocity kmph             72.28
%   mileph                                           45.17
% Max extended relative velocity    kmph             144.56
%   mileph                                           90.35
% Frame time (total)    ms                           1.984
% Frame time (active)   ms                           1.536
% Range FFT size    -                                256
% Doppler FFT size  -                                32
% Radar data memory required    KB                   272
% Velocity resolution   m/s                          1.25
% Velocity resolution (m/s per 2D-FFT bin)  m/s/bin  1.25
% Velocity Maximum  m/s                              20.08
% Extended Maximum Velocity m/s                      40.16
% Maximum sweep accorss range bins  range bin        0.85
% 
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 5 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
lowPower 0 0
profileCfg 0 60.25 568 7 53.57 0 0 70 1 224 4915 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
frameCfg 0 1 16 0 100 1 0
guiMonitor -1 1 0 0 0 0 0
cfarCfg -1 0 0 8 4 4 0 1280 1
cfarCfg -1 1 0 4 2 3 1 1280 1
multiObjBeamForming -1 1 0.5
calibDcRangeSig -1 0 -5 8 256
clutterRemoval -1 1
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 8.42
cfarFovCfg -1 1 -1 1.0
sensorStart