Team,
My customer noticed that we use very high resistance values for the VCOM pin resistor divider, and they were wondering if there is a reason for that. Do they need to be in the several-MOhm range? The only reason I can think of is to avoid overloading the pin if the VCOM_SEL bit is set to internal.
Also, could they drive the pin with an op-amp or voltage reference instead?
Thanks,
Antonio