Other Parts Discussed in Thread: AWR1642
We are using AWR1642 for short range configuration.
Test scenario : Two adults(one moving away from the radar and another moving towards the radar) are moving with same velocity with a separation of approximately 1.5 metres on x axis.
Observation : When both the adults are at same distance on the Y axis , both the adults are shown as a single tracker.
Query : What is the minimum separation required to show the adults as two trackers ?
Will the separation change in case of vehicles ?
We are processing only trackers in our code since it has Y range and velocity. We understand that there is a velocity resolution factor but we need to test by maintaining the same velocity .