This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: .bin file conversion/interpretation

Part Number: AWR1642BOOST
Hi there,
I am doing experiments on the the EVM for vital signs. I understand that from the developer's guide, that the output of the EVM will be saved as a .bin file in the path lab-0001-driver-vitalsigns\vitalSigns_host\gui_exe. I tried to convert the .bin file saved as output from EVM so that I can view the results however, it is shown as a full text file in the characters (small part) shown below:
    B
 ƒ   rÐRc             €      HUÀI5"  0›>¤¥¼öZ½  ²B lOC‹.ÚB À¨A ÀsAz mA  AÀ
Í@Ë)ã;ï¤ó>Ó…>Ò2;>(HÒFú— B     `ŸA x´B                                   L   Lÿàÿ›ZþüCÿõ ÿ£ÿ;ý×ü¤Ë· wÿ‡û÷ûd0$˜ûÇýØÿþ`ì ¼ ¸ Z œü<þ] }ÿ    B
 „   Ø’ÎSc             €      ˆáÜI5"  øŒ>/ç¼›Œ¾  ²B lOC‹.ÚB À¨A ÀsAz mA  Ašwã@ºˆà;ï¤ó>Ó…>Ò2;>6\G}*B     `ŸA x´B                                   L   Aÿäÿ˜]þ«üQÿíà<ÿ­ÿ#ýÆüÇû¹ }ÿ$ûwû¬ï\5Wûˆý÷ÿOþdß· Å ~ Rüþ%d hÿ    B
 …   šV˜Uc             €      ”ÔI5"  -M,>T”½ˆ§l½  ²B lOC‹.ÚB À¨A ÀsAJ’dA  AÞAHWà;ï¤ó>Ó…>Ò2;>Û01Gj1(B     `ŸA x´B                                   L    ÿçÿ¶VþŒüMÿï5ÿÁÿý„ü»Ý {ÿ@ûªû‰ÉHuû±ý Gþ7Äê ï å M fü&þ;– Pÿ    B
 †   œbWc             €      @šäI5"  Nþ)>0¡½Ëæ>  ²B lOC‹.ÚB À¨A ÀsA|A_A  AÆ}AŒ{å;ï¤ó>Ó…>Ò2;>ЩlGÎVOB     `ŸA x´B                                   L   <ÿàÿžbþ˜üMÿõ×?ÿÛÿývü·'Ý sÿ ûyû¨þn6Rû—ýÞÿ&þZêð ç â N Wü0þQ 9ÿ    B
 ‡ 
 ƒ ÉMI"  °BÔÁˆþé¾22€¾  WB ?C  pB @ÝA @ƒA¶ÖšA  aAP“AA7=‹Aü >‚z«>`ΰ?"h¥Q‚biD     @NA жB                                   L   v ÄOí=Ý·%’ôLæßÖ'+GÜn X÷ðå÷ë ‚µýáú@õÐýÖ¿köñøEñ³œüŒýq‡ EþÐþ»    B
Is there any way that I can view my results or convert it into a C++ or a hexadecimal file? where I will be able to interpret it as format mentioned in the slides “Output packet on UART”.
Thank you,
Amy Amelyn