Other Parts Discussed in Thread: HDC2080, HDC1010, HDC1080
Team, I have received the question below from my customer. Can you help me to address it?
rgds, Eric
We have a problem with a humidity sensor (HDC2010) that has been selected on a design to track the humidity level in a "dry cavity" type meter housing, i.e. a hermetic housing with desiccant, which leads to a humidity level close to zero. It turns out that our tests show abnormally high results of more than 20% RH with a varying offset, which first led us to believe that our boxes had leaks, but after analysis, it is the sensor measurement that is wrong.
If you read the datasheet carefully, you will find the explanation:
We had not paid attention to this point before because the sensor is well suited for a range of 20% to 80%.
Is our analysis the right one, is it the fact that we are always below 20% HR that shifts our measurement? If so, do you have another sensor in your range that is suitable for these conditions (low permanent humidity)?