Hi there,
I am recently working with CAN bus on IWR1642BOOST (V2). I am trying to read signal from RX pin after the CAN transceiver (TCAN1042HGVDQ1) but get nothing when running the CAN driver test coming with SDK. I have made sure that the position of S2 is on "CAN" side. Later, I tried to test the connection and found that the MISO1 and MOSI1 pins are directly connected with Pin 14 and Pin 12 on J5 which is different from Table 1 on Page 7 of the 1642BOOST user guide. Now, it seems impossible to read RX message from CAN transceiver from J6 or J5 connector. I would like to ask whether it is a design mistake. If so, would it be possible to be fixed in the next version?
Thanks,
Xinjun