Hi Sir,
I have a question about TMP432,
For the local channel, it tmp register is 0x00, and for the remote channel 1 is 0x01,
Since these two registers are between to each other,
Can I read two bytes of the register 0x00 to represent the register valus of 0x00 and 0x01?
For the first one byte, is the tmp value of the 0x00, And the second one is the tmp value of the 0x01,
Is this reading action is correct or wrong? Pleas help to advice it, thank you,
Regards,
Samuelson