This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1614-Q1: does the ch-x address increment or decrement automatically

Part Number: LDC1614-Q1

Hello,

My customer is wondering if the addresses of all the channels from ch0 - ch3 increment or decrement automatically without declaring stop condition.  For example, if ch0 is configured, the other data from ch1 - ch3 can be read out without configuring the each address.  I don't think it can be since there is no information shown in the datasheet, but please let me confirm that.

Another question is if my customer needs to configure start-stop conditions each time they read out the each channel?  For example, do they need to configure start - slave address - ch0 address - ch1 address - ch2 address - ch3 address - stop or start - slave address - ch0 address - stop - start - slave address - ch1 address ....?

Best Regards,

Yoshikazu Kawasaki