Part Number: MMWAVE-STUDIO
Other Parts Discussed in Thread: IWR1443
Hello,
I have a hardware configuration of IWR1443 + DCA1400.
After a single Trigger command, DCA1400 is writing raw data as "adc_data_Raw_0.bin" as expected. The data size also matches with the Chirp+Frame configuration. However, if I need to Trigger a new chirp block, I have to arm DCA again, which clears the above mentioned data.
Is there any possibility to trigger multiple chirp blocks and append the new raw data to the same .bin file.
Thanks.