Part Number: IWR1642BOOST
Hi,
I am a student trying to use the IWR1642BOOST for my project. My embedded programming skills are basic so I know I have a steep learning curve especially since I am starting with a complex device like this .
I have a couple questions.
1. Some of the training videos for the mmwave sensors do not work. I contacted TI Support and I was told to post it here. The links are below
training.ti.com/introduction-mmwave-sdk
There are others too but this was the one that was currently giving me issues.
2. Is the IWR1642BOOST EVM the only hardware needed to the out-of-the-box demo or do I need a launchpad as well? I connected it to the computer, also installed the stand-alone XDS drivers as stated by the user guide but my computer still doesn't recognize the COM ports so I am not able to run it on the Demo visualizer.
3. The user guide also says that after connecting the EVM board to power(I used a 5V, 4A AC adapter), the NRST and 5-V LEDs should glow but I'm only getting the red 5V LED to blink, could this mean that there is a problem with my board? (I also tried resetting it by pressing the SW2 switch but no change) Could that be why I am having issues establishing a connection with the EVM and my computer?
Thanks