Other Parts Discussed in Thread: MMWAVE-STUDIO
Hello,
I have thoroughly read the forums and documentation about TDM - MIMO operations on IWR1443EVM Radar (with TSW1400EVM acquisition module).
What we are trying to do, is sent the same chirp (which means that once we have set it up as Profile 0, we will NOT change profile on subsequent transmissions and/or on different TX antennas) on the three antennas available on the board.
Correct me if I am wrong: [on MMWAVE-STUDIO]
**UNDER "CHIRP" SECTION ON THE SENSOR CONFIG PAGE**
we select TX0 with start chirp = 0 and end chirp = 0, then press set - profile id0 [TX0 Enabled, Tx1 and TX2 disabled]
we deselect TX0 and select TX1 with start chirp = 1 and end chirp = 1 - profile id 0 [TX1 Enabled, Tx0 and TX2 disabled]
we deselect TX1 and select TX2 with start chirp = 2 and end chirp = 2 - profile id 0 [TX2 Enabled, Tx1 and TX0 disabled]
Under frame config:
- start chirp TX = 0
- end chirp TX = 2
Is everything correct?
Will we obtain a behaviour like a 12 antenna MIMO (3 Tx * 4 Rx) using this procedure?