This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1101EVM: Win7 installation

Part Number: LDC1101EVM
Other Parts Discussed in Thread: LDC1101

Hello. I try to install LDC1101 EVM GUI under Win7 and, as many others, not really succesfull. It's started with drivers (installation completed but the card is not identified). I checked previous messages in the forum and found that I'm not the the first with that problem. I tried during last two days all suggestions from the past:

- I installed GUI as administrator (the latest version)

- I run it first time as administrator - the card was not identified

- I cleaned everything and repeated installation several times on 2 PCs (both Win7) - result negative

- I applied drivers from the  pack 4810.Fix - at least some progress - the card is appeared and fixed to COM9, however the card is not visible in the GUI

- I reinstalled the soft once more keeping the drivers - COM9 & card is not visible!

- On second PC I got another effect - installation of the NI pack stuck at 52% and quite "hard", after I interrupt installation it shows the message (sorry don't remember exactly), something like "problems with identification of keys or license for Windows Vista (???). After cleaning several times and re-installation with the same result I stopped my attempts.

So, my fantasy is out. Could  somebody suggest some helpfull steps? Please!