This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: CONFIGURATION FOR A DISTANCE OF 150 Meters

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: AWR1642

Hello,

I am using the AWR1642BOOST evaluation module. I had read on one of the threads that range can be increased to more than 150 meters. If it is possible to increase to more than 150 meters please share the configuration. Would like to go up to 200 meters if possible.

Currently, mmWave demo visualizer is being used and following is the configuration details.

% ***************************************************************
% Created for SDK ver:02.00
% Created using Visualizer ver:3.1.0.1
% Frequency:77
% Platform:xWR16xx
% Scene Classifier:best_range
% Azimuth Resolution(deg):15
% Range Resolution(m):0.977
% Maximum unambiguous Range(m):50
% Maximum Radial Velocity(m/s):1.08
% Radial velocity resolution(m/s):0.14
% Frame Duration(msec):1000
% Range Detection Threshold (dB):15
% Doppler Detection Threshold (dB):15
% Range Peak Grouping:enabled
% Doppler Peak Grouping:enabled
% Static clutter removal:disabled
% ***************************************************************
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0 adcCfg 2 1
adcbufCfg -1 0 0 1 0
profileCfg 0 77 432 7 18.24 0 0 10 1 500 16670 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 16 0 17.408 1 0
lowPower 0 1
guiMonitor -1 1 1 0 0 0 0
cfarCfg -1 0 0 225 4 4 0 5120
cfarCfg -1 1 0  64 2 3 0 5120
peakGrouping -1 1 1 1 1 63
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
bpmCfg -1 0 0 1
lvdsStreamCfg -1 0 0 0
nearFieldCfg -1 0 0 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 4 31 0
CQSigImgMonitor 0 31 4
analogMonitor 1 1
sensorStart