Hi,
We are developing 200khZ solution based on pga460 and have a few queries about it.
Our transducer is 200khz. but the device firmware always detects 250kHz. (Sometimes inf). Distance is always static at 1024cm
Please find attached our reference schematic, PCB design and the data sheet of the transducer that we are using.
- we are testing the system on 12 V
- TI recommenced transformer was not available so we have used alternative part previously approved by you.
Following parts are used in the development of solution.
PH9185.013NL (Transformer)
SS320LWHRVG (Diodes)
TLV61064A (Supply @ 12V)
Following is my register settings (I am also writing BPF and LPF using register write command )
14 (TVGAIN0),44
15 (TVGAIN1),44
16 (TVGAIN2),44
17 (TVGAIN3),08
18 (TVGAIN4),64
19 (TVGAIN5),9A
1A (TVGAIN6),99
1B (INIT_GAIN),C0
1C (FREQUENCY),11
1D (DEADTIME),40
1E (PULSE_P1),04
1F (PULSE_P2),86
20 (CURR_LIM_P1),3F
21 (CURR_LIM_P2),D5
22 (REC_LENGTH),03
23 (FREQ_DIAG),00
24 (SAT_FDIAG_TH),EE
25 (FVOLT_DEC),7C
26 (DECPL_TEMP),0F
27 (DSP_SCALE),00
28 (TEMP_TRIM),00
29 (P1_GAIN_CTRL),11
2A (P2_GAIN_CTRL),00
2B (EE_CRC),7A
40 (EE_CNTRL),00
41 (BPF_A2_MSB),E1
42 (BPF_A2_LSB),FF
43 (BPF_A3_MSB),F3
44 (BPF_A3_LSB),72
45 (BPF_B1_MSB),06
46 (BPF_B1_LSB),47
47 (LPF_A2_MSB),7C
48 (LPF_A2_LSB),D3
49 (LPF_B1_MSB),01
4A (LPF_B1_LSB),97
4B (TEST_MUX),00
4C (DEV_STAT0),80
4D (DEV_STAT1),00
5F (P1_THR_0),20
60 (P1_THR_1),00
61 (P1_THR_2),22
62 (P1_THR_3),22
63 (P1_THR_4),22
64 (P1_THR_5),22
65 (P1_THR_6),FC
66 (P1_THR_7),E4
67 (P1_THR_8),62
68 (P1_THR_9),10
69 (P1_THR_10),84
6A (P1_THR_11),20
6B (P1_THR_12),20
6C (P1_THR_13),20
6D (P1_THR_14),20
6E (P1_THR_15),07
6F (P2_THR_0),20
70 (P2_THR_1),00
71 (P2_THR_2),22
72 (P2_THR_3),22
73 (P2_THR_4),22
74 (P2_THR_5),22
75 (P2_THR_6),FC
76 (P2_THR_7),E4
77 (P2_THR_8),62
78 (P2_THR_9),10
79 (P2_THR_10),84
7A (P2_THR_11),20
7B (P2_THR_12),20
7C (P2_THR_13),20
7D (P2_THR_14),20
7E (P2_THR_15),07
7F (THR_CRC),11