This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3DToF System Estimator Tool: Software Maximum Distance Limited to 100m

Other Parts Discussed in Thread: OPT8241

Hello,

I'm using the 3DToF System Estimator Tool and OPT8241 to design a ToF system that needs to be able to reach 200m.  The User Guide says the maximum distance in the program should be 1000m (this info can be found on page 13 under Input Control).  Is there a way the software can be updated to be able to reach a longer distance?  I know that distance is pretty big for the regular emitter, but I'm using my own light source and the FoV is not that big either.

I'm currently designing my system using the 100m limit and can estimate the approximate power needed at 200m (about 4x times more peak power), but I would like some more accurate output numbers (such as FL and aperture) because I will also design my own lensing system.

Thanks in advance,

Andre