Other Parts Discussed in Thread: AWR1843, IWR6843
Hi
I have some questions regarding the A/D of AWR1843 and IWR6843 mmWave Chip since both of them are compatible.
1) What is the correct maximal sampling rate? As in "AWR1843DeviceErrataSiliconRevision1.0" it says that max. sampling rate is 25Msps (real) and 12.5Msps (complex). However in "AWR18xx/16xx/14xx Technical Reference Manual (Rev. C)" unter "3.1.1.1 18xx introduction" it says that max. sampling rate is 18.75Msps. Which info is correct?
2) Is the max. sampling rate dependent on A/D resolution? I.e does it always have 25Msps(real) for all A/D 12-,14-,16-bits ??? If not, how is the dependency between max. sampling rate and A/D resolution?
Thanks very much for helping me with above questions.
Best regards,
Le