Other Parts Discussed in Thread: IWR1642
HI,
am not able flash sdk for iwr1642boost. which sdk version i need to flash. this evm arrived in jan 2019.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
am not able flash sdk for iwr1642boost. which sdk version i need to flash. this evm arrived in jan 2019.
Hi Shann,
An EVM from Jan 2019 should have the production version of IWR1642 chip i.e. ES2.0 which is compatible with MMWAVE-SDK 2.1.0.4. The EVM comes pre-flashed with the SDK demo which you can run using the mmWaveDemoVisualiser as explained in the SDK users guide unless you flashed some other binary onto it, in which case you can re-flash the SDK demo (refer to the SDK users guide). Please also refer to the following thread.
Thanks
-Nitin