Other Parts Discussed in Thread: AWR1642,
Hello,
I have a quick question regarding the number of LVDS lanes of the AWR1443 as compared to AWR1642.
While the AWR1642 has only two differential data out lanes (Lane 0 and Lane 1), the AWR1442 incorporates two additional lanes (Lane 2 and Lane 3) with the signal names HS_RESERVED_TXP[2], HS_RESERVED_TXM[2], HS_RESERVED_TXP[3] and HS_RESERVED_TXM[3] as indicated in the datasheet.
Do these two additional lanes provide any further information and does it make sense to route these onto a debug connector as well? Or is it possible to read out all relevant data using only Lane 0 and Lane 1?
Best regards,
Johnny