Other Parts Discussed in Thread: LMT84, TMP235
Many greetings to All,
I've honestly done my best to research this before asking this question... That said, I am using an Arduino UNO to program an ATtiny85 microprocessor to read an LM35C and light an LED based on ranges of the LM35C. My main question is, "How do I configure the LM35C so that I get the Celsius temperature ranges below 2C. I see several circuit diagrams on the Internet pertaining to this, but there is no consistent solution; hence, I figured I'd ask the experts. Relevant information might be that I am using the ATtiny85 in it's basic form, with the 1MHz speed--not 8MHz.