Other Parts Discussed in Thread: IWR6843, UNIFLASH,
Tool/software: Code Composer Studio
Using the IWR6843 in the 50m People counting LAB19. Attempting to load the binary LRPC_lab_xwr68xx.bin. Using the XDS110 interface. Have com Data at COM3 and Uart at COM4 in device manager.
After loading 90% of the demo I get "[ERROR] Cortex_R4_0: File Loader: Verification failed: Target failed to write 0x0007FF00". Power cycled the board several times. Also had the XDS110 interface detect that it needed a code update and performed the update. Same error.
Of course verification attempt also fails.