Other Parts Discussed in Thread: IWR1443, IWR1642, IWR6843, TIDEP-0091
I have a requirement where we need two separate functionalities, one device needs to classify,track and count objects (IWR1642) and the second device needs to measure a liquid level in a container (iwr1443). When it is implemented it will be in two separate locations using separate PCB's.
However for application development.
I am wondering whether a single board/chipset can be used for both these functionalities? or is the level measurement works only with IWR1443? is it because of the antenna design or is it something else specific to the chipset i.e the extra transmitter.
If I need these two functionalities, should I be ordering these two boards separately? or Can the IWR6843 EVM be used to run both these codes?