This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: High-accuracy results are not accurate

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

Hi,team

Thank you very much for your help!

I am using the IWR1443 BOOST for the tank level measurement test. IWR1443 is placed on the top of the tank. The actual height from the top of the tank to the liquid level is 1 meter. I use a high-accuracy experimental project, but I found it fundamentally during the test. I can't measure it. I move IWR1443 horizontally. The result is different every time. The result is between 1.12-1.16. The deviation from the true value is not a fixed value. If the deviation is a fixed value, I can subtract it. However, the deviation is not fixed after each translation. What should I do? Thanks!

In addition, when the liquid level changes, the measurement results increase or decrease as the liquid level rises and falls. That is, the measurement results are different every time the IWR1443 moves horizontally.

The liquid is transparent water.

Best Wishes!

Jacky