This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: demo visualizer and mmwave studio

Part Number: IWR1642

Hello All,

I am using xWR1642 and DCA1000 for my experiments.

I have doppler-range map obtained using specific parameters from mmwave demo visualizer. 

But why am I not able to use the same parameters in mmwave studio ?

For example, in my demo visualizer I see that the Calculated Velocity resolution is 0.2812m. But in mmwave studio&nbsp I cannot configure my velocity resolution to be less than 0.5 (km/h). I would like to know where I am going wrong.