This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-C2000EVM: Is there a way to run two sensors at once?

Part Number: TDC1000-C2000EVM


Is there a way to run two sensors at once? I have a simple tank (like 7.5 x 7.5 cm wide and 25 cm tall) and I would like to place a sensor on the bottom, which is working already, and sensors on the side. The idea is to change the density of the liquid in real time and have the software account for the change in density. The sensors on the side will find the speed of sound in the liquid, and I would like to relay that to the sensor on the bottom to find the liquid level. Is this possible to do with the GUI software provided?