This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWAVE-STUDIO: how to use TestSource in mmWave Studio 2.0.0.2

Part Number: MMWAVE-STUDIO


I want to use TestSource in mmWave Studio 2.0.0.2 with DCA100EVM and IWR1642EVM.

and I have referenced http://e2e.ti.com/support/sensors/f/1023/t/754136.,and I use the same config.

However, in my test, the target set up in TestSource cannot be seen. Here is my result

Is there any guide about how to use Testsource?

  • Hi,

    Please ensure that you configure the test source from the TestSource Tab in mmWave Studio (the default settings are okay to start with, but you need to press the set button on that tab to configure the test source.

    Then, on the SensorConfig tab, under the Frame Configuration, please make sure the "Test Source Enable" checkbox is ticked when you press Set. It should be as in the screenshot below.

    Can you confirm that you have done this?

    Best Regards,

    Anand

  • Hi,
    I am sorry that haven't done before. After do this, it works well.
    Thanks a lot for your help.