This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC2114EVM: Issue with driver

Part Number: LDC2114EVM
Other Parts Discussed in Thread: LDC2114,

Hello,

I download the latest version of the Sensing Solution EVM GUI 1.9.4. But I was not able to connect my LDC2114EVM to the GUI. I tried to upload wrong driver file because there is not LDC2114 driver file included with the GUI software. How can I conncect my LDC2114EVM to my computer?

Where and how can I install the driver? The LDC2114EVM is not connected to the GUI software

I saw the same kind of issue  on the forum but cannot resolve my issue


Thanks

  • Update the driver using the "Device Manager" application on your computer

    -By plugging and unplugging the USB cable, you should be able to identify the USB port that you are using.
    - Right click the port and select properties, then "Update driver"
    - Tell the application to search this folder for the driver: C:/ti/Sensing Solutions EVM GUI-1.9.4/EVM Driver

    There is only one driver for the sensing solutions GUI. It is not LDC2114 specific.
  • Hello,

    Sorry but I made a mistake in my previous message, I mean the firmware and not the driver. So where and how can I install the right firmware?

    Thank you
  • Gwendal,

    I just updated the GUI to include the correct firmware again in the "EVM Firmware" folder. It will take a couple of days to finish posting to the web, but it should be available on Wednesday. Please re-download the GUI at that time and you will find the correct firmware.