This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1642BOOST: About people count example

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: UNIFLASH, IWR1642

Tool/software: Code Composer Studio

About people count example:
Using the provided binary in industrial toolbox 3_1_1, the example can detect people and display on the screen.
If the people count example is imported in latest ccs studio and SDK 2_0_0_4 is used, the code compiles and builds without any error generating the binary. The binary generated is, however, has 10 kb approximately extra size than the provided binary in the toolbox.
When this binary is loaded in EVM board using uniflash, the results aren't same.
The software starts running but no people are detected