Other Parts Discussed in Thread: PGA460,
Hello,
I'm planning on using a PGA460 to drive a single transmitter in the development of a bistatic ultrasonic ranging system through solid ice.
The transducer signal should be powerful enough to be read by a sensor up to 13 meters away (a separate system) in roughly this configuration:
I'm planning on using a 40kHz ground sonar transducer like this one:
https://www.steminc.com/PZT/en/mini-bolt-clamped-langevin-transducer-40-khz-no-threaded-hole
The system runs on a collection of large 12V batteries in a remote, harsh environment.
All of the literature I've found about the PGA460 is about relatively low-power transducers and I wanted to check if there are any problems inherently in trying to drive a larger one. The lack of current limiting and tuning capabilities of most of the commercially available equipment (such as those powering ultrasonic cleaners) has left me seeking alternatives; plus, the development software alongside the BOOSTXL-PGA460 looks very helpful in the design stages.
I have not yet determined the exact power needed to transmit the signal, but a quick calculation gives the following (I don't expect to require close to the full 30W):
Resonant frequency = 40kHz +/-.7kHz
Resonant impedance =< 25 ohm
Any comments or would be highly appreciated - I am new to ultrasonics! Is there a more suitable product?
Many thanks,
Chris