This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: using XDS560 (Blackhawk USB560 v2 System Trace) emulator instead of XDS110

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

Hello,

Using EVM IWR1443Boost demo board, I’m debugging in functional mode (SOP[2:0] = 001) with the TI debug image flashed. However XDS110 is not able to perform a real reset of the system and I keep pushing the reset button for restarting SW otherwise CCS reset crashes the SW.

Fortunately I have a Blackhawk USB560 v2 System Trace and DevPack board readily available.

It seems to me the DevPack is more tailored for use with radar studio and pre-built binaries than as a generic debug help.

Can you please provide some guidance for using them to enter a real debug mode on the IWR1443 Boost (with SOP[2:0] = 011)?

(with DevPack or other (HD connector adapter?), doesn't matter)

Thanks and best regards,
Loic