Other Parts Discussed in Thread: DRV5056, DRV5055
Tool/software: WEBENCH® Design Tools
We are building a gas level monitoring system and using an analog hall effect sensor for detecting the level.
For the test purpose, the following mechanism is used,

The magnetic flux density changes when the lever position goes up and down.
We have tried measuring the magnetic flux density using DRV5053 but we are not getting many variations in the output voltage. The value range is between 0.97 to 1.028V. With this, we are unable to map the gas level.
Can anyone please suggest an analog Hall effect sensor for the above application.