This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: SPI MISO multiplexing in cascaded design

Part Number: AWR1243

Hi!
We are designing cascaded radar with 4 AWR1243P.
My question is about SPI MOSI output of AWR1243P. We want to use multislave SPI bus for this design like scheme below.

We want to multiplex MISO line by 4 AWR1243P.
It is specified in datasheet that MISO has pull up.
But what is the state of the MISO of AWR1243P when CS of High (chip unselect)? If state is low communication will fail.
Can this state be controlled? Or we need to use separated SPI buses?

  • Hi

    I have contacted the hw cascade team to answer this question

    Thank you
    Cesar
  • Hi Igor,

    The default SPI pull resistor state does not change based on chip-select state. So MISO would still have a weak pull-up applied by the device during SPI transfers. The internal pull resistors will be close to 100kohm. This should enable the line to be driven to whatever state the selected device need to drive it to. I don't see a problem there.

    However, for cascaded operation, if your application requires frequent reprogramming of the profile, chirp or frame configuration, I would suggest designing with dedicated SPI masters for each AWR device to help reduce SPI command latency bottlenecks.

    Thank you,
    -Randy
  • Thank you
    I was just confused by the low state of MISO in the time chart of Radar Interface Control Document.