This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Range-Azimuth Heatmap Data Format Demo Visualizer

Part Number: AWR1642


Hi,

With the supplied TLVParser.py script, range FFT data that has been recorded can be written to a txt.

mmw Demo Data Structure_8_16-7.pdf indicates a structure tag at the beginning of each TLV structure.

The script uses struct.unpack for each packet section (range, azimuth, stats,....)

The data sequence of the heat map is: R1[0],R2[0],R3[0],R4[0],R5[0],R6[0], R7[0], R8[0], R1[1],R2[1].....R1[255],R2[255],R3[255],R4[255]

From %MMWAVE_SDK_PATH/packages/ti/demo/xwr16xx/mmw/docs/doxygen/html/index.html under 'Azimuth static heatmap':

'The antenna data are complex symbols, with imaginary first and real second' as so:

Imag(ant 0, range 0), Real(ant 0, range 0),...,Imag(ant N-1, range 0),Real(ant N-1, range 0)

Initially this is used for range profile and should work with heatmap, considering Rx, Real, Imag.

struct.unpack('H', data[2*i:2*i+2])

However, the output before doing any uint to int conversion and assigning antenna appears to be somewhat false.

e.g.: 46, 137, 32, 65507, 65315, 233,65465, 65453, 65452

How must the structure tags from the pdf be implemented? How should the struct.unpack(format, buffer) input be configured?

Is there a way to get the heatmap plot data directly/ how does Demo Visualizer process the data?

Regards