I am evaluating DRV401 for developing a residual current sensor. I want to use a ungapped ring core as the probe to avoid magnetic unblance caused by multiple primary conductor, but I find it hard to choose a proper core because the DRV401 probe drive power is limited and the working frequency is high. A ring core with high permeability means high inductance, which is hard to be saturated by DRV401. Can I use a external circuit like push-pull to amplifier the voltage and current of probe? In such way it can be easier to drive probe core into saturated with a high frequency.