This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Some question of AWR1843 BOOST

Part Number: AWR1642
Other Parts Discussed in Thread: AWR1843BOOST, MMWAVE-SDK, MMWAVE-STUDIO

Dear Sir,

1. According to the data, the bandwidth of 1843 can be up to 4GHz. Can the bandwidth be set to 1GHz when using AWR1843BOOST?

2. When using AWR1843BOOST, can 3 Tx be turned on or off independently, such as 1 Tx on and 2 Tx off?

3. What type data can AWR1843BOOST output?What type of interface is the output?

4. What are the development suites (both software and hardware) that come with AWR1843BOOST?

  • Hi,

    Some of your questions have been answered in other thread-

    https://e2e.ti.com/support/sensors/f/1023/p/778364/2877350#2877350

    And remaining answers are here-

    3. If you are talking of ADCData of the device, it can either stored and used internally or send externally over LVDS interface. And if you are asking about sending the object result data (processed data from signal processing chain) then there are UART, CAN/CAN-FD, SPI interface which can be used to send output.

    4. Software: mmWave-SDK, TI-Rex, mmWave-Studio (RF Evaluation); Hardware: DCA1000 (to capture raw ADC data over LVDS)

    Regards,

    Jitendra