This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-TDC7200EVM: Different Ultrasonic Flow Sensors, 1MHz

Part Number: TDC1000-TDC7200EVM

Hello, I am trying to use a piezo flow meter sensor (Part number SMFM21F1000) with the TDC1000-TDC7200EVM and I'm not getting any signal in GUI when connected to the EVM. I get a signal using the transducer that came with the kit (Part number SMD10T2R11) but no signal when using the sensor I purchased seperately when put in the same pins with the same GUI parameters as the working one. Can you think of a reason why this would be the case? I've attached links to the specs of both sensors mentioned.

Working sensor:www.steminc.com/.../piezo-ceramic-disc-10x2mm-r-215-khz-wire-leads-smd10t2r111wl

Non-working sensor:www.steminc.com/.../ultrasonic-flow-sensor-1mhz-send-receive

Thanks