This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP432: Temp Sensor Replace by MOSFET

Part Number: TMP432

Dear Team,

Can we replace the remote temperature sensor by MOSFET?

Do you have a suitable MOSFET?

BR

Kevin

  • Hi Kuan,

    We recommend the use of NPN or PNP BJT of the 3904 and 3906 variants.
    2N3904 and 2N3906 are TO-92 package
    MMBT3904 and MMBT3906 are available in various SOT packages
    MMBT3904FA is a 0.6 x 0.8MM DFN
    NST3904 is a SOT-1123
    These last two are similar in size and are the smallest I've seen in the market.

    Thanks,
    Ren