We are using AWR1642 in SRR/USRR configuration
Scenario 1 : Two radar units are placed nearby on field with active Tx antennas, the chirps reflected(chirps of both units ) from the object are received by both the radar units , which then generates IF signal which will be processed . What can be done to avoid processing of the out of phase Rx chirps .
Scenario 2 : Two radar units are placed opposite to each other , the Tx chirps from a radar is received and processed by another radar . How to avoid this scenario ?