This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Is it possible to send CLI command through Ethernet communication?

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: DCA1000EVM, , AWR1642

Hi

I am going to parse data of AWR1642BOOST through Ethernet connection by using DCA1000EVM.

What i am concern is that when using UART connection, there are two ports which are data port and command port.

When using Ethernet connection, is there any method to send CLI command to AWR1642 through Ethernet which are similar that of UART connection?

Thanks

Jinhyeong Kim