Other Parts Discussed in Thread: DCA1000EVM, MMWAVE-SDK
Dear Technical Support,
I am trying to understand better what are the values plotted in the "mmWave demo Visualizer GUI" and I have some questions to ask:
1 - Is it possible to debug an up to date version of "mmWave demo Visualizer" using "GUI composer" in runtime mode? I only have the choice of SDK v2.0 or v2.1 and not SDK v3.0 for the IWR6843ISK that I have.
2 - I am intercepting (in javascript debug mode) the values in processRangeNoiseProfile() to get the rp values ("Relative Power" points plotted in the demo chart). Is the bytevec vector of data below is the one stored in the TLV file when user clicks on "Record" button to store the data into a file? If yes then It would be easier for me to get these values reading the file instead of copy/pasting them in debug mode.
Snapshot of "mmWave.js" file:
3 - Are the TLV values the Point Clouds? I understand that according to the type of the TLV values, I can get either Point Clouds (in cartesian coordinates) or raw information from radar processing: do you confirm?
4 - Related to question 3, can I get (or read) the ADC samples in debug mode? If yes, where are they? Note that I do not have the DCA1000EVM for the moment cause I am evaluating the needs.
Thanks for your support.
Best regards.
Anthony.