This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3002: What is the spectral response of OPT3002 in the wavelength range 1000nm to 1100 nm

Part Number: OPT3002


Hi All,

Can anybody share the spectral response for OPT3002 in the wavelength range 1000 nm to 1100 nm.

Regards,

Santosh

  • Hi Santosh,

    We do not take data past 1000nm, but you'll see near 1000nm the response is quite low so likely response above drops off further. What is your application and the reason for asking? Are you trying to measure above 1000nm or worried about interference from those higher wavelengths?

    Best,

    Alex