There are IWR1443 connected to 23K256 SRAM via SPI (master mode)
Needed to transfer 10000 bytes for one session (23K256 supports such SPI "sequence" mode)
SPI clock is 20Mhz, then session latency must be ~5ms.... However, time measure shows >10ms
SPI_MULT_ICOUNT_SUPPORT is on, dma mode switching cause nothing changes.
(Of course, -O1/2/3 compiler options used)
What other way to fix driver or its parameters for speedup SPI transfer ?
Regards.