Part Number: IWR6843ISK-ODS
Other Parts Discussed in Thread: IWR6843ISK, AWR1642
I refer to this link for my understanding of the term "Angular resolution" http://dev.ti.com/tirex/content/mmwave_industrial_toolbox_3_1_1/.metadata/.html/antennas.html
Scene setup
IWR6843ISK-ODS is mounted on the ceiling at a height of 3m.
Since this board has 120 degree field of view in both azimuth and elevation, it simplifies my question.
2 Objects of equal size, for ex: 2 stationary cube shaped boxes of same size and reflective property are placed on the floor. From the field of fiew of the radar, these two boxes are placed in a straight line along one of the axis (X).
Now as per the link above the azimuth angular resolution of IWR6843ISK in Azimuth plane is 15 degrees. And let us assume the azimuth plane is covering the X axis. If so to identify these two boxes as two separate
items.
the centroid of these two boxes have to be separated by (tan 15)*3m = 0.87m (3m is the distance from ceiling to the floor) => is my theory correct?
If the above is correct then if I apply the same concept the distance of separation to identify two objects along the elevation plane is (tan 58) * 3m = 4.8m => as angular resolution is 58 degrees on the elevation
plane
These appear to be large values, considering the fov of the radar from that height may not even extend to these distances. Can some one please clarify what is the correct equation that should be used to calculate the separation
distance between two stationary objects for a MIMO radar when angular resolution is given in degrees.